When Will CodeWarrior Run On Windows Vista?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When Will CodeWarrior Run On Windows Vista?

38,981 Views
FC
Contributor III
Hello,
 
Will there be a patch for CodeWarrior to run on Windows Vista soon?  All new computers come with Vista, I need to upgrade my computer which runs Windows 98SE because CodeWarrior runs very slow on this computer.
 
Thanks
Labels (1)
0 Kudos
Reply
48 Replies

1,922 Views
mauricio2346
Contributor II
Hello
i attempting to run CodeWarrior Development Studio for Microcontrollers V6.0 and Metrowerks Codewarrior IDE V3.0 on my laptop ( under windows Vista basic).  on installation process, y both cases seem to install without any trouble, but, when i try to run (open a proyect, or create a proyect from proyect wizard, the software doesn´t work properly and it closes.  on internet i read about this problem and i found that it should solve removing it from windows firewall, but im still trying What can i do?.    plus, y want to know if CPROG08SZ  Command Line Programmer comes within Development Studio V6.0. (Professional version)

Regards;
Mauricio
0 Kudos
Reply

1,922 Views
J2MEJediMaster
Specialist I
According to the CW for MCUs factsheet here, CW for MCUs 6.2 is compatible with 32-bit Vista. You need to upgrade.

---Tom

0 Kudos
Reply

1,922 Views
Safari
Contributor I

but..... when?.........:smileysad:............when could we have in our machines the updated version that supports Windows Vista O.S. 64 bits?  I bougth a new machine with Vista 64 bits and the only program i used in XP and now I'm trying to use in vista 64b, and I can't,  is Codewarrior V6.2 for microcontrollers I'm Frustrated because I will participate in the SAMART CAR and I think it will be a really big problem.

 

I hope freescale team could solve this problem early....:smileytongue:

 

regards

0 Kudos
Reply

1,922 Views
Andrey
Contributor III
I got my laptop and I downloaded CW V6.0, it runs perfect on Vista. I used it for 12 days now. Seems to be faster, although I'm not sure if it's the laptop or the CW V6.0.

I did not notice any visual/significant changes, except for
- Some difference in adding components
- Yes, skip programing promt checkbox is back (the one that let's you select a programming adapter and other programming options))!

Great job!

p.s. this version still does not work with Windows XP 64-bit. I guess because there is no driver for the device. The installer gives an error and quits.
0 Kudos
Reply

1,922 Views
CrasyCat
Specialist III
Hello
 
  I can confirm that CodeWarrior MCU V6.0 has not been extended to support Windows XP 64-bit.
 
CrasyCat
0 Kudos
Reply

1,922 Views
Curt
Contributor IV
Amen. 
0 Kudos
Reply

1,922 Views
peg
Senior Contributor IV
Yes, "they" seem quite happy to follow Microsoft's lead in dropping support at the older end. But as for the newer end.........
 
0 Kudos
Reply