We bought the Graphic LCD Library driver package for the...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We bought the Graphic LCD Library driver package for the...

2,823 Views
SteveB
Contributor I
We bought the Graphic LCD Library driver package for the KSO7xx family for use with CodeWarrior on 8 bit processors.  The package requires that we define a preprocessor compiler switch, GHW_SINGLE_CHIP (as in #define GHW_SINGLE_CHIP).  I've looked the documentation but have not found where to add this preprocessor compiler switch.  The company supplying the software said the following: "Compiler switches are usually defined on the command line, or if an Integrated Development Environment is used, in some parameter setup window for the compilation project.  Usually definition of compiler switches are located in the IDE near the place where you also can define additional include file paths for use during compilation."
 
We're "stuck in the mud" and can use some help.
 
Steve Baker
Labels (1)
0 Kudos
Reply
1 Reply

1,046 Views
CrasyCat
Specialist III
Hello
 
I need more info to answer your question.
 
- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat
0 Kudos
Reply