Visualization Tool update while running

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Visualization Tool update while running

3,177 次查看
Vicam
Contributor I

I am running a small test program on my DEMO board. I have the value for an analog input mapped to an Analog Instrument in the Visualization Tool, which is great. The problem is that I can’t get the instrument to update its value until the program is halted. I have a breakpoint set and have it automatically continue. I have tried to run a command to update it, but can’t find one. I can run a RD port_name and have it log in the command window. I can also run a INSPECTORUPDATE and have the value update in that window, but nothing updates the instruments in the Visualization Tool until you halt. Do you have any ideas?

标签 (1)
0 项奖励
回复
2 回复数

1,600 次查看
CrasyCat
Specialist III
Hello
 
You can pretty easily perform a periodic refresh of the content of the Visualization component.
 
  - Place the Visualization component in Edit Mode
  - Click with the right mouse button within the visualization window (but outside of any instrument)
  - In the property change Refresh mode to "Periodical" and specify the refresh period.
 
CrasyCat
0 项奖励
回复

1,600 次查看
Vicam
Contributor I
Great. Thank you.
0 项奖励
回复