Using "Hardware Diagnostics"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using "Hardware Diagnostics"

2,140件の閲覧回数
charlesk
Contributor I

Gentlemen:

 

I have a CodeWarrior setup with a Freescale P2020 running and can download and execute the sample test program.

 

The question came up today how to run the hardware diagnostics to check memory in our board. I can open the hardware diagnostics screen, but it errors out when trying to write memory.

 

The "Memory Display" screen works fine and I can change memory values at known memory locations from that screen, just not from the Hardware Diagnostics screen. I am running the same config file and setting up MMU, DDR, LAWBARS and the like the same, but cannot seem to run Hardware Diagnostics.

 

Can someone offer a suggestion or two to help move forward.

 

Charles Krinke

ラベル(1)
0 件の賞賛
返信
1 返信

1,609件の閲覧回数
charlesk
Contributor I

let me reply to my own post as I have some additional data.

 

I can use the menu option Debug->EPPC->Fill Memory and fill memory with 8, 16 & 32 bit values for at least the first 1MByte of RAM space. So, I know the Fill Memory is working, but just not the Hardware Diagnostics menu item.

 

 

Charles Krinke

0 件の賞賛
返信