Using Codewarrior in a Virtual Environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Codewarrior in a Virtual Environment

3,001件の閲覧回数
WillemEradus
Contributor I

Hi.

 

I'm using CW using Parallels (is similair to VMWARE, it allows you to run XP on OS X). After a few glitches CW is working fine but I can't program my devices using the ML-12 (USB Multilink). It connects to the device (it even did an upgrade of the firmware) but it 'loses' connection when I debug / flash the micro-controller. Running it from my laptop with 'native' XP works fine.  

 

Any one of you guys usingf CW and ML in a virtual environment ? Tips / Clues .....

 

Cheers, Willem. 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,924件の閲覧回数
RichardB
Contributor I

Hi Willem

 

Did you manage to fix your issues with CW in Parallels?  I'm thinking of trying the same thing soon...

 

Thanks!

 

Richard

 

0 件の賞賛
返信

1,924件の閲覧回数
WillemEradus
Contributor I

Hi Richard,

 

I left Parallels and moved to VMWARE fushion (2.0.6) on Leopard this is working flawlessly on my iMac. I suggest you download a trial of either version and see if it works for you (or not)

 

Cheers, Willem. 

 

0 件の賞賛
返信

1,924件の閲覧回数
CarlFST60L
Senior Contributor II

We use VMware for all our stuff with codewarrior and have no real problems.

 

Good luck.

0 件の賞賛
返信