Undefined : "__HEAP_START" Undefined : "__mem_limit" Undefined : "__stack_safety"  link failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Undefined : "__HEAP_START" Undefined : "__mem_limit" Undefined : "__stack_safety"  link failed

ソリューションへジャンプ
1,740件の閲覧回数
changxychang
Contributor I

I am using Code Warrior 7.2 and building for the  54418 CPU, with MQX V3.7

 

I have ported some existing code over and fixed a bunch of compile errors. I am now stuck on some linker errors. I realise because the code uses malloc() and free() I need to define a heap.

 

 

Error   : Undefined : "__HEAP_START"

Referenced from "__break" in

Error   : Undefined : "__mem_limit"

alloc.c line 176   Referenced from "brk" in

Error   : Undefined : "__stack_safety"

alloc.c line 176   Referenced from "brk" in

Link failed.

 

 

 

I have no idea how to fix the problem with  "__mem_limit"  and "__stack_safety" variables

 

I have now removed all my app code and get the same link error.

 

I have tested a new project piece of code from MQX 3.7

 

 

Just adding the lines

 

#include <stdlib.h>

 

char *ptr;

ptr = malloc(1000)

 

triggers the link errors, Take out the malloc line, and link error goes away

 

 

 

 

 

 

 

 

Undefined : "__HEAP_START" Undefined : "__mem_limit" Undefined : "__stack_safety"  link failed

I would appreciate any help on this problem, thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,235件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

All these variables are defined in the linker parameter file.

Attached you will find an example using the malloc function.

Rename it to 7_2.zip.

Please have a look to the \lcf\MCF54418_CONSOLE_INTERNAL_RAM.lcf file

Hope this will help you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,236件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

All these variables are defined in the linker parameter file.

Attached you will find an example using the malloc function.

Rename it to 7_2.zip.

Please have a look to the \lcf\MCF54418_CONSOLE_INTERNAL_RAM.lcf file

Hope this will help you.

0 件の賞賛
返信