Unable to debug MRAM Ext Debug on Tower 52259

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to debug MRAM Ext Debug on Tower 52259

1,670件の閲覧回数
accutime
Contributor III

I am CodeWarrior 7.2 with MQX 3.6 along with a Tower MCF52259 CPU and TWRMEM card that contains a 512K MRAM.

 

The jumpers on the MCF52259 board and TWRMEM are set to default.

 

I am using the onboard Coldfire V2-V4 JM60 OSBDM debugger

 

I can build the Web_hvac_twrmc52259.mcp in codewarrior to int_flash_debug , erase and program the internal flash and debug the project without any problem.

 

If I build the project to ext_mram_debug the code is uploaded to the mram and the debugger is entered at __main.

 

I can single step lots of instructions but as soon as I enter RUN I get the message

 

GDI Protocol Plugin

"The debugger cannot read memory"

 

Can anyone help

 

Kind Regards

 

Paul H

ラベル(1)
0 件の賞賛
返信
1 返信

1,163件の閲覧回数
Awera
Contributor III

I have the same problem. Can anyone help me wiht this problem?

 

Thanks

0 件の賞賛
返信