USBWiggler with CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBWiggler with CodeWarrior

3,987 Views
kn
Contributor I
Hi,
    I am using Freescale Code Warrior v 8.2 with DSP56F805. I just bought a USBWiggler (from Macraigor systems) for debugging purposes. Even though the Wiggler is properly connected (verified using the JTAG ScanChain Analyzer, OCD Commander and USBDemon Finder), Code Warrior is not able to recognize it and a connection cannot be made. We have used a parallel port wiggler with Code Warrior and it works fine with it. Is there a way to make the usbwiggler work with code warrior? Do I need any patch or plugin to make it work?
Any help will be highly appreciated,
Thanks in advance,
-KN

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,704 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
The USBWiggler is not supported by CodeWarrior.
In fact it was never tested.
We support the USBTap.
For details, please refer to the link:
 
Regards
Pascal
 
0 Kudos
Reply

1,704 Views
kn
Contributor I
Thanks for the Clarification. We have returned USBWiggler and bought USBTAP.
0 Kudos
Reply

1,704 Views
trytohelp
NXP Employee
NXP Employee
your welcome.
0 Kudos
Reply