USBWiggler with CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBWiggler with CodeWarrior

3,985件の閲覧回数
kn
Contributor I
Hi,
    I am using Freescale Code Warrior v 8.2 with DSP56F805. I just bought a USBWiggler (from Macraigor systems) for debugging purposes. Even though the Wiggler is properly connected (verified using the JTAG ScanChain Analyzer, OCD Commander and USBDemon Finder), Code Warrior is not able to recognize it and a connection cannot be made. We have used a parallel port wiggler with Code Warrior and it works fine with it. Is there a way to make the usbwiggler work with code warrior? Do I need any patch or plugin to make it work?
Any help will be highly appreciated,
Thanks in advance,
-KN

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,702件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
The USBWiggler is not supported by CodeWarrior.
In fact it was never tested.
We support the USBTap.
For details, please refer to the link:
 
Regards
Pascal
 
0 件の賞賛
返信

1,702件の閲覧回数
kn
Contributor I
Thanks for the Clarification. We have returned USBWiggler and bought USBTAP.
0 件の賞賛
返信

1,702件の閲覧回数
trytohelp
NXP Employee
NXP Employee
your welcome.
0 件の賞賛
返信