USB to Parallel converter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB to Parallel converter

4,988件の閲覧回数
Kabous
Contributor I
Hi,

I am trying to use a USB to parallel converter for the communication between my PC and DSP. It has got no connectivity.  What should I do?

Thanks
Kabous
ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,034件の閲覧回数
Kabous
Contributor I
Hello,

The problem is that the USB to parallel converter is listed under USB connections in device manager.  It is not linked to the LPT port.  Anyone got an idea how to link the USB to the LPT1 port.

Thanks
Kabous
0 件の賞賛
返信

2,034件の閲覧回数
J2MEJediMaster
Specialist I
I would assume that the convertor would come with some sort of driver that you would install on the host computer. This driver would mimic a parallel port in the host system and redirect all I/O sent to this "port" to the USB port. Did the convertor come with a software disc?

---Tom
0 件の賞賛
返信

2,034件の閲覧回数
Kabous
Contributor I
Yes it did came with a driver but it is only for windows 98 and me. Windows XP is plug and play. I went to speak with a few guys  and they told me that the usb to parallel converters is dedicated for printers and is not seen as an LTP port.

The only solution is to use a Parallel to PCMCIA card or a docking station.

Thanks anyway
Kabous
0 件の賞賛
返信

2,034件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
The connection must be stable. An USB/Parallel converter will not work.
 
Regards
Pascal
0 件の賞賛
返信