USB TAP serial number

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB TAP serial number

3,298 Views
jimwilliams57
Contributor I

I am trying to connect more than one USB TAP to my PC and then select which to use when debugging with Codewarrior Classic.  The Remote Debugging->Edit Connection dialog seems to allow for this, but requires I enter the "USB TAP Serial Number (hex)".  Where do I find the serial numbers of my USB TAPs?

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

2,939 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

It should be written on the backside of the USBtap.

But also, you can find from ccs console typing next commands:

(bin) 59 % dele a

(bin) 60 % findcc utaps

USB TAP Serial Numbers:

  10261530

10261530

Regards,

Marius

0 Kudos
Reply

2,939 Views
jimwilliams57
Contributor I

Thank you.  That solved the problem.

A note to anyone trying to do this, the serial number must be entered as a hex number (with the leading 0x).  For example, one of mine has the serial number 12022118.  It must be entered 0x12022118.

0 Kudos
Reply

2,939 Views
trytohelp
NXP Employee
NXP Employee

Hi,

To give you right answer, can you please provide me the dev tool used.

To do that you must:

  Under CodeWarrior IDE (classic)

      Start the IDE and click on Help | About Freescale CodeWarrior.

      Click on Installed Products 

      Provide us all info displayed.

      Or you can save them in a txt file.

  Under Eclipse IDE

    1-      Start Eclipse and click on Help ¦ Freescale Licenses

      The Status column gives the status of the license.

      Under Product, select it and click on details.

      A new dialog show up giving license details.

      Provide us all info displayed

    2-      Start Eclipse and click on Help ¦ About CodeWarrior Development Studio

      Under Installed Products, you will see the version used.

Regards

Pascal

0 Kudos
Reply

2,939 Views
jimwilliams57
Contributor I

I can't find hot to attach a file, so here is everything from CodeWarrior Classic:

Installed Products:

  CW Dev Studio, Power Architecture, Professional Edition, v8.8.3, Build 90619

  CW Dev Studio, Power Architecture, Professional Edition, v8.8.4, Build 100924

  CodeWarrior Development Studio for Power Architecture v8.8.6 Build 121029

  CW Dev Studio, Power Architecture v8.8.x, Service Pack 2 for 8569, Build 1350

  CW Dev Studio, Power Architecture, Professional Edition, v8.8, Build 80229

  CW Dev Studio, Power Architecture, Linux Applications Edition, v8.8, Build 80229

  CW Dev Studio, Power Architecture, Debugger Data Drop, v8.8.3, Build 0810

  CW Dev Studio, Power Architecture v8.8, Service Pack 2 for P1011, P1012, P2010, and MPC8569, Build 100907

  CW Dev Studio, Power Architecture v8.8.x, Service Pack 1 for P1011, Build 1350

  CW Dev Studio, Power Architecture v8.8.x, Service Pack 1 for P1012, Build 1350

  CW Dev Studio, Power Architecture v8.8.x, Service Pack 1 for P2010DS, Build 1350

  CW Dev Studio, Power Architecture v8.8.x, Service Pack 1 for P2010RDB, Build 1350

IDE Version: 5.9.0 Build 2529

Plugins: 113

================================================================================================

ASINTPPC.dll             5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:02 AM       628K     

================================================================================================

================================================================================================

CmdIDE.exe               5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:19 AM       41K      

================================================================================================

================================================================================================

IDE.exe                   5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:16 AM       10.23M   

================================================================================================

================================================================================================

IDENewDialog.dll         5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:03 AM       201K     

================================================================================================

================================================================================================

IDE_MFC60cw.dll           6.00.8665.0               6.0.8665.0               6.0.4.0                   5/17/2009, 11:56 PM       1.59M    

================================================================================================

================================================================================================

IDE_MSL_DLL90_x86.dll     5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:54 PM       296K     

================================================================================================

================================================================================================

InstallHelperKeys.exe     No Version Info           0.0.0.0                   0.0.0.0                   3/22/2005, 4:01 AM       76K      

================================================================================================

================================================================================================

lmgr8c.dll               No Version Info           0.0.0.0                   0.0.0.0                   5/2/2005, 4:09 AM         832K     

================================================================================================

================================================================================================

MWCore5_0.dll             5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:57 PM       236K     

================================================================================================

================================================================================================

MWRADUtils.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:03 AM       260K     

================================================================================================

================================================================================================

Mwregsvr.exe             5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:05 AM       36K      

================================================================================================

================================================================================================

MWRegSvrWinApp.exe       5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:06 AM       36K      

================================================================================================

================================================================================================

PluginLib.dll             5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:54 PM       120K     

================================================================================================

================================================================================================

PluginLib2.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:54 PM       120K     

================================================================================================

================================================================================================

PluginLib3.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:54 PM       120K     

================================================================================================

================================================================================================

PluginLib4.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:54 PM       84K      

================================================================================================

================================================================================================

PluginLib5.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:55 PM       84K      

================================================================================================

================================================================================================

PluginLib6.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:55 PM       84K      

================================================================================================

================================================================================================

runhelper.exe             1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:07 AM       4K       

================================================================================================

================================================================================================

SHW32.DLL                                         4.0.1.0                   4.0.1.0                   2/10/2000, 11:15 AM       110K     

================================================================================================

================================================================================================

tcl84t.dll               8.4.12                   8.4.2.12                 8.4.2.12                 9/25/2006, 7:22 AM       576K     

================================================================================================

================================================================================================

xerces-2_2_0.dll         2, 2, 0                   2.2.0.0                   2.2.0.0                   5/18/2009, 12:05 AM       2.14M    

================================================================================================

================================================================================================

Bin\Plugins\COM

================================================================================================

  PackAndGo.dll             1,0,0,0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:09 AM       344K     

  SaveRestoreRegisters.dll 5.7.0.0                   5.7.0.0                   5.7.0.0                   5/18/2009, 2:05 AM       180K     

  ObjectInspector.dll       5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:17 AM       332K     

  DebugDatabase.dll         5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:27 AM       284K     

  EPPCStationeryWizard.dll 8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:02 AM       254K     

  DebugRegisterMgr.dll     5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:28 AM       112K     

  CommandWindow.dll         5.9.0.2529               5.9.0.2529               5.9.0.2529               5/18/2009, 12:22 AM       1016K    

  ExternalBuildWizard.dll   5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:33 AM       60K      

  TipOfTheDay.dll           1,0,0,0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:08 AM       64K      

  LoadSaveFill.dll         5.8.0.1170               5.8.0.1170               5.8.0.1170               5/18/2009, 2:05 AM       174K     

  HardwareDiagnostics.dll   5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:25 AM       2.09M    

  FlashProgrammer.dll       5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:25 AM       5.60M    

  LogPoint.dll             5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:22 AM       56K      

  VariableFormatter.dll     5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:23 AM       52K      

  TracePointOn.dll         5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:23 AM       52K      

  PausePoint.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:22 AM       100K     

  MWActivate.dll           5.9.0.2529               5.9.0.2529               5.9.0.2529               5/18/2009, 12:19 AM       600K     

  SkipPoint.dll             5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:23 AM       52K      

  ScriptPoint.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:23 AM       116K     

  TracePointOff.dll         5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:23 AM       52K      

  TraceDataStorage.dll     5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:23 AM       128K     

  SoundPoint.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:23 AM       56K      

  CPPCodeCompletion.dll     5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:18 AM       808K     

================================================================================================

Bin\Plugins

================================================================================================

================================================================================================

Bin\Plugins\Compiler

================================================================================================

  ppc_eabi_libimporter.dll 4.3 155                   4.3.0.155                 4.3.0.155                 5/11/2009, 10:49 AM       97K      

  Cc_ppclnux.dll           5.8.0.1170               5.8.0.1170               5.8.0.1170               5/18/2009, 2:06 AM       125K     

  Im_ppclnux.dll           5.8.0.1170               5.8.0.1170               5.8.0.1170               5/18/2009, 2:07 AM       97K      

  OsekCompiler.dll         2, 1, 2, 0               2.1.2.0                   2.1.2.0                   9/12/2006, 2:00 PM       75K      

  ppc_eabi.dll             4.3 155                   4.3.0.155                 4.3.0.155                 5/11/2009, 10:45 AM       3.06M    

  Asm_ppclnux.dll           5.8.0.1170               5.8.0.1170               5.8.0.1170               5/18/2009, 2:07 AM       103K     

  ppc_eabi_asm.dll         4.0.0                     4.3.0.155                 4.3.0.155                 5/11/2009, 10:41 AM       357K     

  PCLintCompiler.dll       1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         80K      

================================================================================================

Bin\Plugins\Debugger

================================================================================================

  TcpIpComm.dll             5.9.0 Build 0000         5.9.0.0                   5.9.0.0                   5/18/2009, 2:05 AM       13K      

  TRKFraming.dll           5.9.0 Build 0000         5.9.0.0                   5.9.0.0                   5/18/2009, 2:05 AM       12K      

  SerialComm.dll           5.9.0 Build 0000         5.9.0.0                   5.9.0.0                   5/18/2009, 2:05 AM       13K      

  StabSymbolics.DLL         5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:20 AM       156K     

  DisassemblerPPC.dll       8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:05 AM       140K     

  Dwarf2Symbolics.DLL       5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:21 AM       280K     

  DwarfSymbolics.DLL       5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:19 AM       224K     

  EPPCPlugin.dll           8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:01 AM       965K     

  MWSerialWin32.dll         1.1 build 006             1.1.0.6                   1.1.0.6                   5/18/2009, 2:05 AM       13K      

================================================================================================

Bin\Plugins\Debugger\protocols

================================================================================================

  EPPC_CCSProtocol.dll     8.8.0.100903             8.8.1.35367               8.8.1.35367               9/3/2010, 1:10 PM         487K     

  EPPCAbatronProtocol.dll   8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:03 AM       158K     

  EPPCLinuxTRKProtocol.dll 8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:09 AM       267K     

  EPPCCodeWarriorTRKProtocol.dll 8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:03 AM       139K     

================================================================================================

Bin\Plugins\Debugger\rtos

================================================================================================

  EPPCrtos_OSEK.dll         2, 0, 0, 0               2.0.0.0                   2.0.0.0                   5/18/2009, 2:06 AM       332K     

  LinuxInfo.dll             2, 0, 0, 19               2.0.0.19                 2.0.0.19                 5/18/2009, 2:09 AM       161K     

================================================================================================

Bin\Plugins\Linker

================================================================================================

  ExternalBuildLinker.dll   5.9.0.2529               5.9.0.2529               5.9.0.2529               5/18/2009, 12:33 AM       80K      

  Ln_ppclnux.dll           5.8.0.1170               5.8.0.1170               5.8.0.1170               5/18/2009, 2:06 AM       123K     

  PCLintLinker.dll         1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         84K      

  BatchRunnerPreLinker.dll 1.0.0 Build 6             1.0.0.6                   1.0.0.6                   5/18/2009, 2:06 AM       41K      

  ppc_eabi_linker.dll       4.3 155                   4.3.0.155                 4.3.0.155                 5/11/2009, 10:48 AM       862K     

  PostLn_ppclnux.dll       5.8.0.1170               5.8.0.1170               5.8.0.1170               5/18/2009, 2:07 AM       98K      

  BatchRunnerPostLinker.dll 2.0.0 Build 8             2.0.0.8                   2.0.0.8                   5/18/2009, 2:05 AM       41K      

================================================================================================

Bin\Plugins\Preference Panel

================================================================================================

  PEPPCTarget.dll           8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:03 AM       90K      

  PDebugx86Except.dll       5.9 Build 2529           5.8.0.0                   5.8.0.0                   5/18/2009, 12:35 AM       64K      

  PBatchRunnerPreLinker.dll 1.0.0 Build 5             1.0.0.5                   1.0.0.5                   5/18/2009, 2:05 AM       30K      

  PBatchRunnerPostLinker.dll 2.0.0 Build 6             2.0.0.6                   2.0.0.6                   5/18/2009, 2:05 AM       45K      

  PCLintSettings.dll       1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         82K      

  PCLintOptions.dll         1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         41K      

  OsekPanel.dll             2, 1, 2, 0               2.1.2.0                   2.1.2.0                   8/29/2006, 6:11 PM       70K      

  PFrontEndC.dll           5.9 Engineering Build     5.8.0.0                   5.8.0.0                   5/11/2009, 10:49 AM       68K      

  PGnuAssembler.dll         1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:07 AM       50K      

  PGnuCompiler.dll         1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:07 AM       54K      

  PGnuDisassembler.dll     1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:07 AM       51K      

  PGNUEnvVars.dll           1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:08 AM       50K      

  PGnuLinker.dll           1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:08 AM       49K      

  PGnuPostLinker.dll       1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:08 AM       50K      

  PGnuTarget.dll           1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:08 AM       54K      

  PGnuToolCommand.dll       1.0.0.0                   1.0.0.0                   1.0.0.0                   5/18/2009, 2:08 AM       65K      

  pMWCVS.dll               1.3.0.2529               1.3.0.2529               1.3.0.2529               5/18/2009, 12:34 AM       64K      

  pmwSourceSafe.dll         5.5.1.40704               5.5.1.40704               5.5.1.40704               4/8/2004, 1:37 PM         29K      

  PPPCDebuggerSignals.dll   MW_VERSION_STR_VAL       1.1.0.1170               1.1.0.1170               5/18/2009, 2:04 AM       37K      

  PPQ3TraceBuffer.dll       5.9 Engineering Build     5.8.0.0                   5.8.0.0                   5/18/2009, 2:04 AM       96K      

  PPreprocessorC.dll       5.9 Engineering Build     5.8.0.0                   5.8.0.0                   5/11/2009, 10:49 AM       72K      

  PRConnCCS.dll             1.0.0.2 b002             1.0.0.2                   1.0.0.2                   5/18/2009, 2:04 AM       84K      

  PRConnPowerTapPRO.dll     8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:03 AM       49K      

  PRConnUSBTap.dll         1.0.0.00                 1.0.0.0                   1.0.0.0                   5/18/2009, 2:04 AM       50K      

  prfEABIasm.dll           4.3 Build 155             4.3.0.155                 4.3.0.155                 5/11/2009, 10:50 AM       36K      

  prfEABIcodegen.dll       4.3 Build 155             4.3.0.155                 4.3.0.155                 5/11/2009, 10:50 AM       82K      

  prfEABIdisasm.dll         4.3 Build 155             4.3.0.155                 4.3.0.155                 5/11/2009, 10:50 AM       34K      

  prfEABIglbopt.dll         4.3 Build 155             4.3.0.155                 4.3.0.155                 5/11/2009, 10:50 AM       33K      

  prfEABIlinker.dll         4.3 Build 155             4.3.0.155                 4.3.0.155                 5/11/2009, 10:50 AM       74K      

  prfEABIlinkeropts.dll     4.3 Build 155             4.3.0.155                 4.3.0.155                 5/11/2009, 10:50 AM       31K      

  prfEABIproject.dll       4.3 Build 155             4.3.0.155                 4.3.0.155                 5/11/2009, 10:50 AM       52K      

  PSerialComm.dll           5.9 Engineering Build     5.8.0.0                   5.8.0.0                   5/18/2009, 2:03 AM       29K      

  PSourceFolderMapping.dll 5.9 Engineering Build     5.8.0.0                   5.8.0.0                   5/18/2009, 2:04 AM       52K      

  PSyscallSettings.dll     5.8.0.1170               5.8.0.1170               5.8.0.1170               5/18/2009, 2:04 AM       36K      

  PTargetConsole.dll       1.0.0.1170               1.0.0.1170               1.0.0.1170               5/18/2009, 2:04 AM       34K      

  PTcpIpComm.dll           5.9 Engineering Build     5.8.0.0                   5.8.0.0                   5/18/2009, 2:04 AM       22K      

  PWarningC.dll             5.9 Engineering Build     5.8.0.0                   5.8.0.0                   5/11/2009, 10:49 AM       68K      

  PExternalBuild.dll       1.0.1.0                   1.0.1.0                   1.0.1.0                   5/18/2009, 12:33 AM       64K      

  PDebuggerPICSettings.dll 1.2.3.777                 1.2.3.777                 1.2.3.777                 5/18/2009, 2:04 AM       50K      

  PDebugEPPCExcept.dll     8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:03 AM       48K      

================================================================================================

Bin\Plugins\Support\Common\Comm_IO

================================================================================================

  PP_TargetAccess.dll       5.8.0.2529               5.8.0.2529               5.8.0.2529               5/18/2009, 12:24 AM       60K      

================================================================================================

Bin\Plugins\Support\Common

================================================================================================

================================================================================================

Bin\Plugins\Support

================================================================================================

  CPlusSourceGen.dll       5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:17 AM       272K     

  MWComBase.dll             5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:01 AM       64K      

  MWComHelpers.DLL         5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:59 PM       460K     

  MWRadModel.dll           5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:03 AM       572K     

================================================================================================

Bin\Plugins\Support\Flash_Programmer\File_IO

================================================================================================

  BIN_File_IOEngine.dll     5.8.0.2529               5.8.0.2529               5.8.0.2529               5/18/2009, 12:24 AM       26K      

  ELF_File_IOEngine.dll     5.8.0.2529               5.8.0.2529               5.8.0.2529               5/18/2009, 12:24 AM       21K      

  SREC_File_IOEngine.dll   5.8.0.2529               5.8.0.2529               5.8.0.2529               5/18/2009, 12:24 AM       34K      

================================================================================================

Bin\Plugins\Support\Flash_Programmer

================================================================================================

================================================================================================

Bin\Plugins\Support\PowerPC_EABI\Abatron

================================================================================================

  bdiifc32.dll             V1.42                     1.0.4.2                   1.0.4.2                   8/14/2006, 7:04 AM       115K     

================================================================================================

Bin\Plugins\Support\PowerPC_EABI

================================================================================================

================================================================================================

Bin\Plugins\Support\PowerPC_EABI\USBTAP\redist

================================================================================================

  wdlib.dll                 7.00                     7.0.0.0                   7.0.0.0                   5/2/2005, 10:27 AM       60K      

  wd_utils.dll             7.00                     7.0.0.0                   7.0.0.0                   5/2/2005, 10:27 AM       108K     

================================================================================================

Bin\Plugins\Support\PowerPC_EABI\USBTAP

================================================================================================

================================================================================================

Bin\Plugins\Support\PowerPC_EABI\USBTAP\util

================================================================================================

  wdreg.exe                 No Version Info           0.0.0.0                   0.0.0.0                   5/2/2005, 10:27 AM       128K     

================================================================================================

Bin\Plugins\version control

================================================================================================

  mwcvs.dll                 1.3.0.2529               1.3.0.2529               1.3.0.2529               5/18/2009, 12:34 AM       228K     

  mwSourceSafe.dll         1.0.3.716                 1.0.3.716                 1.0.3.716                 4/8/2004, 1:37 PM         137K     

  VCSClearCase.dll         1.1.2.1999               1.1.2.1999               1.1.2.1999               8/16/2004, 1:18 PM       76K      

================================================================================================

Bin\resource

================================================================================================

  CPlusResources.dll       5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:16 AM       24K      

  EPPCStatWizResources.dll 8.8.0.1170               8.8.0.1170               8.8.0.1170               5/18/2009, 2:02 AM       6K       

  ExternalBuildResources.dll 5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/18/2009, 12:33 AM       6K       

  IDEAuxiliaryResources.dll 5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:58 PM       44K      

  IDEResources.dll         5.9.0 Build 2529         5.9.0.2529               5.9.0.2529               5/17/2009, 11:58 PM       52K      

0 Kudos
Reply