USB TAP - ONCE for MC56F8346 using 56800E Flash programmer sw.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB TAP - ONCE for MC56F8346 using 56800E Flash programmer sw.

2,865件の閲覧回数
NanosecPeter
Contributor I

Hi,

 

I have small production run of 50 boards. I was successfully programmed 46 of them using the USB TAP Once, but 4 failed to program. Here is the error message:

 

>>Connected to local CCS server at PORT 41475
>>Configured to use CodeWarrior USB TAP
>>Placing the device into debug mode, please wait...
>>CCCSClient::ResetToDebug: Network timeout

 

What can be wrong?

Thanks,

Peter

ラベル(1)
0 件の賞賛
返信
1 返信

1,160件の閲覧回数
barbara_johnson
NXP Employee
NXP Employee

Hi Peter,

 

This is the StarCore for DSPs forum. Please post your question to this forum.

CodeWarrior for 56xxx DSC

0 件の賞賛
返信