Target settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Target settings

4,322件の閲覧回数
NewProgrammer
Contributor I
Hi,
    I have projects for 2 targets(7119 and 8101) in a  directory and want to run the project for the targets on a machine where these two target boards are connected.The issue is that since both the target boards are connected to the PC using individual  USB TAP's when I debug say 7119 project am not able to download the executable to the board.Is there any way out where I could download the executable to the appropriate board when debugged.
 
Thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,193件の閲覧回数
CrasyCat
Specialist III
Hello
 
  According to your message I assume you are using CodeWarrior fot StarCore. Am I right?
  Then I assume you are trying to connect to 2 distinct board through 2 separate USBTAP. Am I right?
 
  Which version of CodeWarrior are you using?
  To retrieve that info:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
CrasyCat
 
0 件の賞賛
返信

2,193件の閲覧回数
NewProgrammer
Contributor I
Hi,
   I know that I can specify the USB TAP serial no. of the target baord in the target settings of the project.Apart from that is there any alternative.
 
Thanks
0 件の賞賛
返信

2,193件の閲覧回数
CrasyCat
Specialist III
Hello
 
Basically I would recommend you to use 2 distinct remote connections in the IDE Preferences panel.
make sure to specify distinct Port number and USBTAP serial number for each of them.
 
Then in the target setting dialog, Remote Connection panel, select the appropriate connection.
As far as I know this is the only way you could get that working.
 
CrasyCat
0 件の賞賛
返信

2,193件の閲覧回数
NewProgrammer
Contributor I
Hi,
     Thanks for the reply .Yes I am using CodeWarrior for starCore Verion 3.0.0 .Is there a solution for this problem.
 
Thanks
0 件の賞賛
返信