Subgroups in Board for different CW versions?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Subgroups in Board for different CW versions?

7,104 Views
hwrobel
NXP Employee
NXP Employee
Would it be possible to split the board again into PPC/8-bit/16-bit etc as on the old MW community? it would simplify usage a lot.

Heinz
Labels (1)
0 Kudos
Reply
3 Replies

2,652 Views
mikegas
Contributor I
Hey.. neat. didnt know bout this forum till now..  Is there a 32-bit board?
0 Kudos
Reply

2,652 Views
Alban
Senior Contributor II

Hi Mike,

No 32-bit board now coz you need mods for it :smileywink:
You also need peep from FSL to spend some time on them to help.

You're putting your name on the list ??!?
I'm sure Admins will be reading your post ! :smileyvery-happy:

Alban.

0 Kudos
Reply

2,652 Views
marc_paquette
Contributor V
I agree that it would make these forums more manageable. I'll pass your request along to the IT team and keep you posted.
 
Marc.
0 Kudos
Reply