Stopping a command file in True-Time simulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stopping a command file in True-Time simulator

3,067件の閲覧回数
Cmux
Contributor II

I have written a command file to log my variables every 10ms. I am running that command file in an infinite loop. How do I stop the execution of the command file when I want to stop logging data? The only way I found is to kill the true-time simulator application but I am looking for an elegant way to do that.

 

-- 

Cmux

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

1,637件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Cmux,

 

I assume you use HiWare true-time simulator (8/16bit).

REPEAT-UNTIL and WHILE-ENDWHILE loops can be ended by pressing Esc key.

 

Stanish

0 件の賞賛
返信

1,637件の閲覧回数
Cmux
Contributor II

Is there no way to stop an infinite loop?

 

-- 

Cmux

0 件の賞賛
返信

1,637件の閲覧回数
CrasyCat
Specialist III

Hello

 

I assume you are referring to an infinite loop defined in a debugger command file?

Am I right?

 

Then the next question is which processor are you targeting (HC08, HC12, Coldfire, ...)?

Which version of CodeWarrior are you using?

To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.

 

CrasyCat

0 件の賞賛
返信

1,637件の閲覧回数
Cmux
Contributor II
Yes I am referring to an infinite loop in the debugger command file. I am using an MC9S12P microcontroller with CodeWarrior v5.0.
0 件の賞賛
返信

1,637件の閲覧回数
CrasyCat
Specialist III

Hello

 

Did you try to click inside of the command window and press ESC?

This should stop execution of the currently executed command file.

 

CrasyCat

0 件の賞賛
返信

1,637件の閲覧回数
Cmux
Contributor II

Yes I tried pressing Esc in the command window. I tried all sorts of escape sequences in the command window to no avail. Any other ideas?

 

-- 

Cmux

0 件の賞賛
返信