Standalone 56800E flash programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Standalone 56800E flash programmer

7,194 Views
jag
Contributor IV
Hi,
I noticed a problem using the 56800E flash programmer for programming the 56F8013 chip using JTAG via parallel port.
I'm using CW 7.3.

The problem is this one: if I program the flash all works correctly. When I try to Verify the flash it gives me an error, and the chip is frozen until I reprogram it.

This is the log of the programming:

Using Configuration File: C:\Programmi\Metrowerks\CodeWarrior\M56800E Support\initialization\56801x_flash.cfg

Reading File C:\goofy.elf.S...

S-record ID: PROGRAM&DATA

Connecting to CCS...

Connected to local CCS server at PORT 41475

Configured to use Parallel Command Converter at port LPT1

Placing the device into debug mode, please wait...

Flash unit #0 (P:0x000000-0x001FFF) programmed, 7054 words written

Flash unit #0 (P:0x000000-0x001FFF) Verification Passed CRC32 (0xc055cb14)

Exiting Debug Mode...


and this of the verification:

Using Configuration File: C:\Programmi\Metrowerks\CodeWarrior\M56800E Support\initialization\56801x_flash.cfg

Reading File C:\goofy.elf.S...

S-record ID: PROGRAM&DATA

Connecting to CCS...

Connected to local CCS server at PORT 41475

Configured to use Parallel Command Converter at port LPT1

Placing the device into debug mode, please wait...

Flash unit #0 (P:0x000000-0x001FFF) Verification Failed CRC32 (0x690b37d3) expected (0xc055cb14)

Verification Failed

So why the verification is not working?

Thanks Bye Jack



Labels (1)
Tags (1)
0 Kudos
Reply
6 Replies

2,664 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
I don't know if we could investigate it via the forum.
Can I suggest you to log this problem in CRM system ?
So Technical Information Center could invstigate it.
 
Please provide us the application.
Be aware that lot of customers met problem with the parallel interface and Windows OS.
To avoid it, we recommend you the USBTap interface.
 
I don't remember a problem with the flash programmer and the DSP7.3.
The DSC 8.0 and a patch 8.1.1 are available.
There is a free version.
Can I suggest you to try with this version ?
May be this will fix the problem.
 
See below more info.
You can download the DSC 8.0 on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247
There is a patch for the DSC8.0 (must be installed in first) DSC8.1.1
You can download it on our web site via the link:
 http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
Pascal
 
0 Kudos
Reply

2,664 Views
jag
Contributor IV
Hi,
thanks for the answer.
2 thing:
1) the USBtap costs 500$, the parallel JTAG dongle 50$...I need to say something else?

2) I've a quastion about CW 8. There is a issues porting projects from CW 7.3 to CW 8.x? And using 8.x projects with CW 7.3?

Because I work with HC908 too, and porting projects from the old version of CW (3.1) to the new one (CW5.1) is a nightmare, so I decided to not update for the moment.

Bye Jack
0 Kudos
Reply

2,664 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
You're right the USBTap is more expensive than the parallel cable.
Since Windows NT, the parallel port is not anymore managed really by Windows.
So lot of customers meet connection troubles with the parallel port.
To avoid them the USBTap has been introduced.
 
I'm sorry but what is the parallel JTAG dongle ?
We support 3 interfaces:
 - sample parallel cable (parallel on host and board),
 - wiggler interface (parallel on hast and Jtag on board),
 - USBTap (usb on host and Jtag on board).
The wiggler is manufactured by Macraigor. The price is $150.
For details please visite their web site:
 
The USBTap is sold $249.
 
You should move your application to the new DSC tool without problem.
However I can not certify this because this depends directly of your application.
To avoid problem we recommend to backup the project before to move it to the new version.
If you will meet problem you can back to the old version without problem.
 
Regards
Pascal
 
 
0 Kudos
Reply

2,664 Views
jag
Contributor IV
Hi,
I use a parallel to JTAG interface from Axiom Manufactoring, is like the Wiggler.

Bye Jack
0 Kudos
Reply

2,664 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
We support 3 interfaces only:
 - sample parallel cable (parallel on host and board),
 - wiggler interface (parallel on host and Jtag on board),
 - USBTap (usb on host and Jtag on board).
 
We don't support other interface for DSC.
The Axiom board is not supported.
 
Pascal
0 Kudos
Reply

2,664 Views
trytohelp
NXP Employee
NXP Employee
info to log a SR:
 

For Technical Support Issues please use Freescale on line support web page.

- Go to following URL: http://www.freescale.com/TechSupport

- Click on Submit a Service Request. You will come to a login page.

- You can submit your request through the web from there.

0 Kudos
Reply