Segmentation fault on starting PCS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Segmentation fault on starting PCS

1,838 Views
joekawa
Contributor I
I am just an beginner for the Platform Creation Suite.
 
When I excuted the PCS by 'tw', the following message appears.
 
/usr/bin/tw: line 81:  5861 Segmentaion fault   /opt/Embedix/  ...........
 
How can I solve this error?
 
<Environment>
      OS: Redhat 9
      PCS: Platform Creation Suite for Linux OS, V3.01
      Target: M9328MX21ADSE 
 
Thanks.
 
Joe
Labels (1)
0 Kudos
Reply
1 Reply

661 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
Don't know if this problem will be answered on the Forum.
Can I suggest you to log it in the Freescale CRM data base via the web access:
Click on Submit a Service Request.
 
Pascal

Message Edited by Alban on 2007-02-13 03:18 PM

0 Kudos
Reply