SPI and SS Pin problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI and SS Pin problem

1,967件の閲覧回数
Freacky2002
Contributor I
Hi I'm using a  dsp 56f803. My problem at the moment, I need to raise down the SS pin during sending a spi message an then the SS has to be high(nothing to send). I looked in the Processor Expert, but there it seems that I only can set up the SS signal as an Input but not as an output signal. Has anybody expereince in this?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

923件の閲覧回数
ProcessorExpert
Senior Contributor III
Hello,

The MCU does not support automatic SS pin handling, therefore you have to set the "Slave select pin" property to "Disabled" and handle the SS pin using BitIO bean and it's methods.

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 件の賞賛
返信