Running CW 5.2 with P&E USB Multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running CW 5.2 with P&E USB Multilink

1,736 Views
johnthompson001
Contributor II

Is anyone else have problems trying to use Debug when using the P&E USB Multilink and a HCS12 device?

One of the problems seems to be associated with the loading the cmd files.

Example from the Command display:

Loading Target ...

Initializing STARTUP command file:

CMDFILE STARTUP ON "startup.cmd"

Startup Command File execution: startup.cmd

File does not exist: startup.cmd

Startup command file does not exist.

 

 

 

Many thanks 

Labels (1)
1 Reply

1,438 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello John,

Does the P&E hardware is detected by operating system within device manager ?

If not , please refer to this link to install the drivers :

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools... 

Hope it helps

Alice