Regarding USB tap for P2041

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding USB tap for P2041

2,967 Views
asifismail
Contributor I

Hello,

 

We are developing out custom board with P2041, and we are in need of a Codewarrior USB tap for the said processor. When I looked in to the Freescale website, I could find only Codewarrior TAP which connects via both USB and Ethernet. We are looking for a USB tap alone.

 

We also have a Codewarrior tap with P/N : CWH-UTP-CF-HE. Is there any extra probes or connectors that can attach P2041 processor to this CW tap?

Labels (1)
0 Kudos
Reply
6 Replies

2,642 Views
trytohelp
NXP Employee
NXP Employee

Hi Asif,

in the past, most of the time the interface is dedicated to an architecture.

This was the case for CodeWarrior USBTap.

Several versions were available for DSC, Coldfire, etc ...

      http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152102726E4D6E4E3

Now some interfaces are common and can be used on different architectures.

This is the case for P&E Multilink Univeral / FX interfaces.

These interfaces can be used on Freescale HCS08, HC(S)12(X), S12Z, RS08, ColdFire V1/+V1, ColdFire V2-4*, Qorivva 55xx/56xx, and Kinetis ARM microcontrollers.

For details have a look to:

      http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137

there are other interfaces ...

      CodeWarrior TAP

            http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152102726E4D6F994

      CodeWarrior Gigabit TAP

            http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152102726E4D6E4D9

Regards

Pascal

0 Kudos
Reply

2,642 Views
asifismail
Contributor I

Thank you very much it was a valuable information

0 Kudos
Reply

2,642 Views
addiyi
NXP Employee
NXP Employee

Hi,

Codewarrior USB TAP are obsolete and have been replaced with Codewarrior TAP, which as you said have both USB and Ethernet connection. Also, you will also need a probe tip targeted for Power Architecture (P2041 in your case). You must acquire CWH-CTP-COP-YE (Power Architecture® processor ( COP ) Probe Tips for CodeWarrior TAP) .

Adrian

0 Kudos
Reply

2,642 Views
asifismail
Contributor I

Dear Adrian,

Thanks for that information.

Is there any available probe that fits CWH-UTP-CF-HE to connect with P2041 processor?

0 Kudos
Reply

2,642 Views
addiyi
NXP Employee
NXP Employee

CWH-UTP-CF-HE is intended for ColdFire (Microcontroller products), and your board is powered by a PowerArchitecture CPU (P2041).


Adrian

0 Kudos
Reply

2,642 Views
asifismail
Contributor I

Thank you very much

0 Kudos
Reply