Recognition codewarrior usb2serial adapter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recognition codewarrior usb2serial adapter

4,672件の閲覧回数
Ronaldo
Contributor I
Hi,
 
I have an OMEGA  usb2serial adapter to program mcu`s from my laptop. What have I to do to recognize it codewarrior IDE? I downloaded version 5.0 from freescale, and I try to in to MON08 mode, but I coudn´t find in software any option to recognize this adapter.  Any help for this problem is very helpful to me.
 
Thanks.
 
 
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,883件の閲覧回数
jorge
Contributor II

  Ronaldo,

  In my own experience some of RS-232 to USB adapters don't handle some of the control lines of the DB9 adapter (RTS, CTS, etc). Unfortunately, the adapter's manufacturer says the device is fully compatible with the serial port (!!).

  Solution: to get a new, really full compatible adapter.

  Any one in this forum could recommend a model?

0 件の賞賛
返信

1,883件の閲覧回数
peg
Senior Contributor IV

Hi Jorge,

Unfortunately brands don't mean much with this sort of stuff. A lot of times the "brand" is the company that took the device from the crate from China and put it in the hanger pack. My one (that I haven't tested) doesn't have anything written on it but I know it handles the handshake lines to some extent.

BR Peg

 

0 件の賞賛
返信

1,883件の閲覧回数
peg
Senior Contributor IV

Hi Ronaldo,

The PC operating system handles the integration of the USB to serial converter so that it just looks like another COM port to applications. Older OS's may need a driver installed that comes with the adapter.

So Codewarrior doesn't have to know, sshhh!

Having said that the chances of it working are not very good as these adapters are not very good at implementing the short BREAK's used by the MON08 protocol.

BR Peg

 

0 件の賞賛
返信