RAM initalization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAM initalization

2,592件の閲覧回数
NZ_Design
Contributor I
I have external RAM on my system. It is being automaticaly intialized when the system starts up. It is battery backed.

I whish it not to be altered. I are assuming there is a setting to stop this from happening. But where is it.

The memory is decleared as such

c file
#pragma DATA_SEG __GPAGE_SEG BATTERY_RAM
  volatile Prog_Layout   Program[MAX_PROGRAMS + 2];

prm file
      BATTERY_RAM       INTO  NO_INIT     0x200000'G TO 0x3FFFFF'G;   // CS1 BatteryRAM;

yet when the system is rebooted it has 64 in every byte.


anyone got any surgestions.


ラベル(1)
0 件の賞賛
返信
1 返信

1,093件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Are you sure it the compiler startup code which inits your RAM?
I would guess it is something else, the NO_INIT should stop the linker from init your data, and also the startup code would 0-init it, and not write 0x40.
So I would guess that something in your battery backed RAM setup is not working properly and look in that direction.

Daniel

0 件の賞賛
返信