Question regarding mac instructions for CodeWarrior IDE 5.0.9 compiling for the MCF5275

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question regarding mac instructions for CodeWarrior IDE 5.0.9 compiling for the MCF5275

2,226件の閲覧回数
zedraic
Contributor I
Greetings all,

I am working on writing an FIR filter for the MCF5275 and I am attempting to utilize the emac. I have obtained the DSP library from Freescale (DSPLIPUMSW); however, when I compile the the FIR filter code or when I write my own "mac" instructions like "asm("mac.w %d0.l, %d1.l, <<, %ACC0") I get the following error:

Error   : C:\DOCUME~1\rr\LOCALS~1\Temp
\ccQ9aaaa.s : Assembler messages:

Error   : syntax error -- statement `mac.w %d0.l,%d1.l,<<,%ACC0' ignored
ccQ9aaaa.s line 130  

all the other assembly I have written it compiles but it gets stuck on each mac instruction. 

I am using the CodeWarrior IDE 5.0.9 to do the compilation.  I am compiling for use in uClinux on the MCF5275 using the CodeSorcery toolchain that I obtained from Evaluation: CodeWarrior for ColdFire, Linux Application Edition (Windows) download.

If anyone has suggestions/ideas of how to make this work I would greatly appreciate them.

Thanks,
ラベル(1)
0 件の賞賛
返信
1 返信

992件の閲覧回数
J2MEJediMaster
Specialist I
I would suggest that you submit a service request for that. You'll need to provide the source code and the project that you're working with.

To submit a service request, click here.
0 件の賞賛
返信