Program Flash above 0x20000 on 56F8366

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program Flash above 0x20000 on 56F8366

2,819件の閲覧回数
tim_robbins
Contributor I
I am using a 56F8366. My code size has recently jumped above 0x20000, which is about half way thru the total program space. Its also a transistion point from the first 256k space to the other 256k space.
Everytime my software tries to execute an instruction in the code space about 0x20000 I get a illegal op code interrupt. After further review, it appears that its writing all zeros to anything above 0x20000 instead of my code.
 
Any one have any ideas? I am using CW 8.1.1a
 
Thanks,
Tim
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,323件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
I'm not sure but it could be similar to another problem we investigated 2month ago for another chip.
Can I suggest you to log this issue in the Freescale CRM system ?
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
 
Can you please add the following info :
 - do you use Processor Expert ?
 - do you meet the problem in simulator too?
 
Pascal
0 件の賞賛
返信

1,323件の閲覧回数
Mika
Contributor I
Hello!

What was the solution? I am having very similar problems with 56F8345 and CW 8.0. Problems start immediately after program flash size reaches 50%. First I had problems with function pointer array initializations and now I have new weird problem that I haven't been able to kill yet. And I am not using PE.

- MiT
0 件の賞賛
返信