Processor Expert tab is empty

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert tab is empty

6,957件の閲覧回数
Hawkeye
Contributor III
We have 3 developers working on a project and are using a VCS.  After I got the latest copy of the project files the Processor expert tab was empty.  The other developers do not have this problem.
We are using version 7.3 of CodeWarrior 56800/E with ROHS USBTAP update.
 
Any suggestions?
 
Thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
7 返答(返信)

3,366件の閲覧回数
CrasyCat
Specialist III
Hello
 
Just need more info here.
In the original post you say that you are using a VCS.
I assume you mean that you are checking source file in and out in a Version control software before you start building an application.
 
Which files are you checking in?
Just want to make sure you are checking the appropriate ProcessorExpert files to retrieve all information.
 
CrasyCat
0 件の賞賛
返信

3,366件の閲覧回数
sricker
Contributor I
I am interested in knowing which files from a project should be in VCS.
0 件の賞賛
返信

3,366件の閲覧回数
CrasyCat
Specialist III
Hello
 
I would say:
  - All C and assembly source files
  - All header files included there
  - The linker command file (.lcf)
  - The exported project .xml file. Instead of placing the .mcp file (which is a binary file) into your
     VCS system, I would recommend you to export the project to a .xml file (using menu entry
     File -> "Export Project"). This is an ASCII text file and can be easily checked in/out.
  - The ProcessorExpert configuration file (.G_C). This is an ASCII text file containing internal information
    about the Processor Expert project generation.
  - The ProcessorExpert Project file (.pe). This is an ASCII text file containing a description of
     the beans included in your project with their properties.
 
That should be it.
 
CrasyCat
0 件の賞賛
返信

3,366件の閲覧回数
sricker
Contributor I
CrazyCat,
This means exporting the project as .xml each time you wish to commit, correct? I have been using the .mcp file with CVS without issue (so far) but I understand it would be better as xml.
 
Thanks,
Shawn
0 件の賞賛
返信

3,366件の閲覧回数
Hawkeye
Contributor III
Jumping back a few posts - I had a working project, got a new version of the .pe file and the problem occurred.  Freescale quickly responded to an SR and said to re-install Metrowerks.  This solved the problem.
 
The discussion on which files to archive is helpful. We have archived the mcp file but since SourceSafe does not allow multiple checkouts of a binary file we let it get out of date. We shall now switch to the xml format.
 
Thanks
 
0 件の賞賛
返信

3,366件の閲覧回数
CrasyCat
Specialist III
Hello
 
Well my point with checking in the .xml file is that some VCS software are limited or do not allow checking in/out binary files easily.
Also when you are checking a binary file in, you just have the raw binary and you do not see what has changed there between the two versions.
Meaning retrieving differences in project settings from a .mcp file will be impossible.
It is possible for a .xml file.
 
Note that if you check the .xml file you have to import it in CodeWarrior to convert it to a .mcp file again.
CodeWarrior can process only .mcp files.
The xml is just here to get a human readable file containing project settings.
 
At the end of the day it is up to you to decide whether you want to check a binary or a .xml file.
 
CrasyCat
0 件の賞賛
返信

3,366件の閲覧回数
oskay
Contributor I
The same thing has happened to me several times. I suspect that the only solution is to not use Processor Expert. It's simply not trustworthy since this can happen-- ever. I like to contrast this behavior with that of my code in C, which is easily backed up and doesn't just disappear!

The only thing that I've been able to do is use very few of the PE "features" so that it's faster when I have to rebuild the project from scratch.
0 件の賞賛
返信