Problems starting MPC8280

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems starting MPC8280

3,281 Views
Gonzi
Contributor I
Hi,
 
I´m working with a MPC8280 (a Power Quick II) using Codewarrior Development Studio V8.1.
 
I have some problems to find the .h (something like mcp8280.h or mcp82xx.h) for my target.
 
Where can I get this file?
 
Thanks
 
Labels (1)
0 Kudos
Reply
3 Replies

1,553 Views
CrasyCat
Specialist III
Hello
 
I assume you are looking for register definition file for the MPC8280.
We do not deliver these header files as part of CodeWarrior.
 
Not sure whether they are available on Freescale web some other place...
 
CrasyCat
0 Kudos
Reply

1,553 Views
Gonzi
Contributor I
Oh, I´m sorry...
 
You are rigth, I´m looking for register definition file for the MPC8280.
 
I don´t find nothing in Freescale web. I will continue with my search.
 
Regards,
 
Gonzi
0 Kudos
Reply

1,553 Views
Alban
Senior Contributor II
Thread locked as new thread started by the user in the MCUCOM board.
We thank members not to crosspost or post the same question multiple times or in multiple boards.
This divides the replies and causes more work for people who want to answer.
Alban.
0 Kudos
Reply