Problem with srecLoad

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with srecLoad

4,087件の閲覧回数
jeypi
Contributor I
Hello,
 
I'm working with DSP56F8346 and CodeWarrior version 5.6. I'm trying to load my application using the Srec program but the Srec fails and displays the message: Loading Time: 223468ms. First, I loaded the bootloader to DSP56F8346 using JTAG. Then I execute the command: srecLoad -i:COM1 -s:myApplication.elf.S -b:115200 -l:log.txt. Is there any problem with bootloader or the S file need any change? I read the SCI/CAN Bootloader user manual and did every step to load an application but it didn´t work. Does anybody solve this problem already? 
 
Thanks,
 
João Paulo.
ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,066件の閲覧回数
jeypi
Contributor I
Hello guys,
 
I solved the problem. Instead of using srecLoad, I'm using hyperterminal and the bootloader is working.
 
Jey Pi. 
 
 
0 件の賞賛
返信

2,066件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
Thanks for the feedback.
I don't know the tool version you're using.
 
FYI:
Freescale 56800/E Digital Signal Controllers Version 8.2
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC
For details please have a look in:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC&tab=In-Depth_Tab
In the download tab you can download the Special Edition or the Evaluation.
The Special edition contains the special edition license limited to 32 kb of Code.
If you need another version of the license please contact your local distributor.
You can purchase it directly from the web site too.
We changed the pricing and packaging structure for Codewarrior Tool.
Now there are 4 suites:
 special (free version)
 basic
 standard
 professional
Please refer to the link for details:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127262E703BC5
Go to the www.freescale.com and click on My Freescale.
After you were logged, select CodeWarrior Licensing under MY Secure Application.
In the new dialog you can manage your license file.
Keep in mind you can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
If you're using an old version, please backup your project before to try it with this new version.
If you will meet some compatibility issue you could back to the older version without problem.
Pascal
 
 
0 件の賞賛
返信

2,066件の閲覧回数
jeypi
Contributor I
Thanks for helping Pascal. I'm going to look these links.
 
João Paulo.
 
0 件の賞賛
返信