Problem with connecting DemoBoard through JTAG.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with connecting DemoBoard through JTAG.

2,790件の閲覧回数
Ranjicgnr
Contributor I
Hello..
 
I have a problem with my 56F8013 demo board. I am using code warrior hibrid controller ide. My bad luck i change the setting " Initilize unused GPOI's" as input. Earlier it was uninitilized. After that i cant debugg the pgrogramm using the demo board. Again i changed the setting to uninitilized. then also an error message is comming. It is tellig " the core is not connect".  If i am using some other board which is having 56F8013 it is working. How can i solve this problem. That setting i have changed is there in Proccessor bean. And my JTAG connection is through parrel port.
 
ranji
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,484件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
I suggest you to log your request to the Freescale CRM system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request to create a new one or Manage Existing Service Request.
  - You will come to a login page.
  - You can submit your request through the web from there or view the activities of a SR.
Probably this SR will be handle by several teams CodeWarrior and DSC hardware.
 
Regards
Pascal
0 件の賞賛
返信

1,484件の閲覧回数
Ranjicgnr
Contributor I
thanks.
                 I have send my requiest to them. I am waiting its replay.:smileyhappy:
0 件の賞賛
返信