Problem in installing Codewarrior 10.0 Special Edition on windows XP SP3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in installing Codewarrior 10.0 Special Edition on windows XP SP3

2,263件の閲覧回数
SANTOSHKUMAR
Contributor I

The setup file "CW_MCU_v10.0_Windows_SE.exe" downloaded from the Freescale website, during installation halts giving error message "Error decompressing data! Corrupted installer?" while installing file "C:\Program Files\Freescale\CW MCU v10.0\MCU\Help\PDF\Profiling and Analysis Users Guide.pdf".

 

Then in second attempt i deselected documentation then installation stopped at file "C:\Program Files\Freescale\CW MCU v10.0\analysis\1.1.0\lib\host\vendor\win\omniOrb-4.0.7\OpenSSL.zip"

 

Once again i deselected CodeSoucery option and again installation stopped at file "C:\Program Files\Freescale\CW MCU v10.0\analysis\1.1.0\lib\host\vendor\win\omniOrb-4.0.7\OpenSSL.zip".

 

 Is there some pre-requisites for installation of Codewarrior 10.0 Special Edition ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,714件の閲覧回数
J2MEJediMaster
Specialist I

Is that 32-bit Win XP or 64-bit Win XP? Installations on 64-bit OSes are tricky. You can search some of the topics that discuss how to do this. I have set such topics to "float" to the top of the board so that you can find them easily.

 

---Tom

0 件の賞賛
返信

1,714件の閲覧回数
SANTOSHKUMAR
Contributor I
The OS on which i have tried installing is 32-Bit WIN XP.
0 件の賞賛
返信

1,714件の閲覧回数
J2MEJediMaster
Specialist I

It looks like you have a corrupt download file. I would suggest that you file a service request for this. Click here to do that.

 

---Tom

0 件の賞賛
返信