Problem about  DEMO56F8013KIG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem about  DEMO56F8013KIG

2,552 Views
waicircuit
Contributor I
Hi,
I am using the 56F8013 56F8013 Demo Board Kit for motor control. When i try to connect to the board through Code Warrior IDE, I get the error "CCS Protocol Plugin: Unknown Protocol Error". I had not got this error until last week.



Any help?

Thank you,
waicircuit
Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,333 Views
J2MEJediMaster
Specialist I

That message indicates that the debugger cannot find an interface to communicate with the board.

 

How are you connecting to the board? That is, what hardware probe are you using?

 

Has anything changed in the last week? The computer used to host the debugger? Has a peripheral been added? The probe cable changed (if you're using, say, USB)? Has an evaluation license expired?

 

It could be any number of things.

 

--Tom

 

0 Kudos
Reply

1,333 Views
waicircuit
Contributor I

 

I use Parallel connect to hardware

 

and I have some question

1.how different software between software from website and software kid that we with board receive?

 

2.Do I have problem if use software kid by no licence?

 

3.Do the software has expire date? How can we know the date?

 

Thanks you so much.

0 Kudos
Reply

1,332 Views
J2MEJediMaster
Specialist I

To answer your questions:

 

1) The software that came with the board might be an Evaluation or a Special Edition version. A Special Edition version will be fully functional, except it will have certain limits or restrictions. An Evaluation Edition is fully functional, except its license key will expire over a certain interval. Then it behaves like the Special Edition. The other issue it that the tools that came with the board might be a version or two behind what's on the site. You can download the latest version of the Special Edition and experiment.

 

2) Special Edition software will let you do enough to work on small project to give you an idea if you want to use the tools. Ideally, you'll like them and upgrade to a Standard Edition, :smileyhappy: but the choice is yours.

 

3) I don't know what the expiration date might be, it varies. However, if you do a build and see a message about the license has expired in the Warnings and Errors window, then its obvious the license has timed out. However, an expired license shouldn't disable the debugger interface.

 

The parallel port interface can be fincky at times. Adding a peripheral can drag down a laptop's power level such that the parallel signals become unreliable. However, that would cause flaky operation, and not the connection error message that you're getting. I'd start with checking the debugger settings to see that the parallel iterface is selected and check what printer port it is trying to use. Confirm that this printer port is the default one and active in the system software. These things just don't stop working. Something has changed.

 

---Tom

 

 

 

 

0 Kudos
Reply