Problem CW6.3SE in W7 & Ciclone Pro

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem CW6.3SE in W7 & Ciclone Pro

1,229件の閲覧回数
pablobeccacece
Contributor I

Hello,

Recently CW6.3 install on W7 and install the driver for CYCLONE PRO PE. Everything was installed without inconvenience. The problem is when I want to debug from CW6.3 with CICLONE, this does not appear as an option Connection (via USB)

The driver is properly installed CICLONE (JUNGO LTD Ver. 12.2.0.0)

What can I do?

ラベル(1)
0 件の賞賛
返信
1 返信

1,035件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Pablo,

I see the following on my side:

pastedImage_1.png

P&E proposes several interfaces:

     Cyclone PRO

     Cyclone Universal

    Cyclone Universal FX

     USB Multilink Universal

     USB Multilink Universal FX

    

CW for MCU v6.3 was released in 2010.

The Cyclone Universal, Cyclone Universal FX, USB Multilink Universal and USB Multilink Universal FX

were released after this date.

Please can you refer to the links:

- P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

- P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信