PostBuild with BatchRunner

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PostBuild with BatchRunner

1,484件の閲覧回数
xirxe
Contributor I
Hi, I want to run PreBuild and PostBuild batch files from the IDE. In other projects (HC12) I can choose under Target->Target Settings->Pre-Linker the entry "Batch Runner". But with DSC this entry is missing. But even if I add ".bat" to Target->File Mappings and add my batchfiles to the project nothing happens. How to add it the correct way?
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,233件の閲覧回数
J2MEJediMaster
Specialist I

According to the CodeWarrior MC56F8xxx/MC5685x Family Targeting Manual, the DSP tools do not support pre-linker or post-linker operations. See chapter 4, Table 4.3, "Target Settings Panel Elements".

 

You might be able to do something with the command-line tools.

 

---Tom

0 件の賞賛
返信