Pitfalls of upgrading from 3.1 to 6.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pitfalls of upgrading from 3.1 to 6.1?

2,248件の閲覧回数
JohnnyP
Contributor III
I have CW 3.1 for programming my 9S12 project. I just bought the DEMOJM evaluation kit to evaluate processors "in the continuum" and 6.1 came with it.

Is there any danger installing 6.1? Could it cause my 3.1 not to work? That would be bad, since I program deliverable product with it.

Thanks for your help.

John P
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

805件の閲覧回数
peg
Senior Contributor IV
Hi,

Generally different versions of Codewarrior exist on the same PC without any trouble. I have 3 different versions co-existing quite OK.
Freescale support people generally have even more versions at once.

0 件の賞賛
返信

805件の閲覧回数
bigmac
Specialist III
Hello John,
 
During installation of the new version, make sure that no file extension associations are altered.  Otherwise, a double click on a HCS12 project name may launch the incorrect CW version.
 
Regards,
Mac
 
0 件の賞賛
返信

805件の閲覧回数
JohnnyP
Contributor III
Thank you both very much. Now I can click "Install" without fear.
0 件の賞賛
返信