Creating Libraries Using Codewarrior 8.1 for 56F8037

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating Libraries Using Codewarrior 8.1 for 56F8037

3,962件の閲覧回数
Ansi_Cartman
Contributor I
Hello,
 
I am planning to create my own libraries. I am using CW 8.1 and the DSC I am using is 56f8037. I was able to create a library by changing the target to library. But when I include the compiled library, I am having errors. I cant seem to use it.
 
Does anyone have a reference manual or something that can help?
 
Thank you so much!
 
 
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,090件の閲覧回数
stanish
NXP Employee
NXP Employee
Hi Ansi_Cartman,

Perhaps the existing library project e.g ("c:\Program Files\Freescale\CodeWarrior for DSC56800E v8.2\M56800E Support\msl\MSL_C\DSP_56800E\projects\MSL C 56800E.mcp" ) might help you to configure your own library.

Stanish
0 件の賞賛
返信

2,090件の閲覧回数
Ansi_Cartman
Contributor I
Hi Stanish
 
Thanks,
Ill check this out..
 
0 件の賞賛
返信

2,090件の閲覧回数
Ansi_Cartman
Contributor I
Hi Stanish
 
I was successful in making and using the library that I created.
 
Thank you so much!!!!
0 件の賞賛
返信