PCS for MX21

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCS for MX21

2,312件の閲覧回数
hazmatto
Contributor I
I am trying to get the Platform Creation Suite v3.01 running on linux for development on the MX21ADS platform.
After fixing a typo in the installation script on the CD and recreating the installation media, and backgrading our linux development machine to have compatible libraries, we were finally able to install the PCS and the Linux Board Support Package that came with the development kit.
However, when try and run the Target Wizard, it quits with a message about licensing. We have received a license key from Freescale/Codewarrior, but we can't seem to install the license key. There does not seem to be a license.dat file anywhere or a license manager.
Are we missing something? Or do we just need to find the correct spot in the directory structure (/opt/Embedix) to create a license.dat file with the key in it?

Thanks.
-mat
ラベル(1)
0 件の賞賛
返信
1 返信

1,107件の閲覧回数
hazmatto
Contributor I


hazmatto wrote:
I am trying to get the Platform Creation Suite v3.01 running on linux for development on the MX21ADS platform.
After fixing a typo in the installation script on the CD and recreating the installation media, and backgrading our linux development machine to have compatible libraries, we were finally able to install the PCS and the Linux Board Support Package that came with the development kit.
However, when try and run the Target Wizard, it quits with a message about licensing. We have received a license key from Freescale/Codewarrior, but we can't seem to install the license key. There does not seem to be a license.dat file anywhere or a license manager.
Are we missing something? Or do we just need to find the correct spot in the directory structure (/opt/Embedix) to create a license.dat file with the key in it?

Thanks.
-mat


I just noticed that there is a new release of the imx21 bsp (release date 2006 12-12) which probably runs with the LTIB (open-source version of Platform Creation Suite) so I might not have to solve this problem. Downloading it now.
0 件の賞賛
返信