Overflow in segment¿?¿?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overflow in segment¿?¿?

1,862 Views
Celm0
Contributor I

Hi there... 

 

i'm Working with a  56F801 DSP implemmenting a numeric method which its code is quite large PSOtest.c its a 16 KB file.

 

when i make and try to link to the board i get the next 2 errors : 

 

Link error :  Overflow in segment : .p_Code from section : .ApplicationCode 

segment reserved size is : 0x00001f80 -- overflow of : 0x00000db2

 

and 

 

Link error :  Overflow in segment : .p_Data from section : .ApplicationData

segment reserved size is : 0x000003c0 -- overflow of : 0x0000018c

 

 

would somebody help me with this.. i don't understand why i get this error and how to fix it .. i think that it is a very simple solution but i don't know it ..  

 

Thanks for your help ... 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,175 Views
Dhiman
Contributor I

Dear,

Your Flash memory overflowed please use optimistaion level 4 in smm prom-xram setting

prom means flash xram means ram

0 Kudos
Reply