Optimizing C Compiler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Optimizing C Compiler

2,306 次查看
dlf
Contributor I

Hi.

 

The standard and professional edition of codewarrior for DSCs (56800e) have included an optimizer C compiler.

 

How many the C optimizer is better than compiler without C optimizer. (Maybe any percent or how many times in terms of clock cycles for example??)

 

I carried out some test. Comparing  C code vs. ASM code. In terms of clock cycles, the asm is about twice faster than C.    How would be this relationship using C optimizer?

 

 

****

How can I update my CodeWArrior special edition v 8.2.3 to 8.3?  It is necessary unistall the older version and then install the new 8.3 version? I have not found any patch or update?

*****

 

 

Thanks.

 

 

 

 

Message Edited by dlf on 2010-02-15 05:15 PM
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,332 次查看
jag
Contributor IV

 


dlf wrote:

Hi.

 

The standard and professional edition of codewarrior for DSCs (56800e) have included an optimizer C compiler.

 

AFAIK the special version has the same optimizing C compiler, the only limitation is on code size

 

How many the C optimizer is better than compiler without C optimizer. (Maybe any percent or how many times in terms of clock cycles for example??)

 

just try with or without the optimizations enabled

 

I carried out some test. Comparing  C code vs. ASM code. In terms of clock cycles, the asm is about twice faster than C.    How would be this relationship using C optimizer?

 

whit or whitout the optimizations enabled.

You have to enable them in the project preferences (there should be a slide, for different level of optimization).

 

****

How can I update my CodeWArrior special edition v 8.2.3 to 8.3?  It is necessary unistall the older version and then install the new 8.3 version? I have not found any patch or update?

*****

 

You can download and install the new version in parallel of the olders.

 

Thanks.

 

You're welcome.


Bye Jack

 

0 项奖励
回复