Objective-C -- Still supported?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Objective-C -- Still supported?

2,515件の閲覧回数
Frotz
Contributor III
Hello!

I've been evaluating the MCU's and the CodeWarrior IDE for a software-heavy hardware project. I'm very familiar with Objective-C and find it to be a very powerful OO language. It's also very light-weight since it's a very thin layer upon C. For these reasons I'd like to use it for development on this project.

According to the "C Compliers Reference version 3.2", the objective_c pragma is available. Not having an IDE yet, nor having settled on a MCU even, I've not tested this in practise!

Is there anyone who can verify if ObjC works and if so, which MCU's it applies to?

Thank you very much,
Andre.
ラベル(1)
0 件の賞賛
返信
1 返信

1,094件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hello,
 
This problem has been reported to Support team in CRM.
The SR number 1-345621333 has been logged for this issue.
 
Pascal
TIC-CodeWarrior
0 件の賞賛
返信