Object files location..

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Object files location..

2,205 Views
MagnusD
Contributor I

Hi,

I am rookie on Codewarrior, and have a problem.

Where are the object files located?

I created a project, added the file I need to have compiled for the processor, selected and right clicked the file i need compiled, selected compile. No errors everything ok, however I can't locate the object files. 

In the project an empty folder called ObjectCode is created under RAM or internal_FLASH, sooo where is the files?

I only need object code, since I am to handover that to another to link.

Links to good tutorials are very welcome.

Thanks in advance

Magnus 

Labels (1)
0 Kudos
Reply
3 Replies

1,583 Views
J2MEJediMaster
Specialist I

What is the type of CodeWarrior that you are using and its version number?

 

---Tom

0 Kudos
Reply

1,583 Views
MagnusD
Contributor I

The version is professional for MPC55XX version 2.6 build 100423.

Says CWA-PRO-NL on package.

It might be an license issue.

When i registered it, the download page was corrupted.

So I downloaded the "CW55xx_v2_6_Build_100426SE.exe" and appended the license file created to the licence file in root folder.

But I am still not sure if it's because I do something wrong...?

0 Kudos
Reply

1,583 Views
stanish
NXP Employee
NXP Employee

Hello MagnusD,

 

I'd suggest you to see the forum thread below:

 

https://community.freescale.com/message/16758#16758

 

 

Stanish

0 Kudos
Reply