OSEK RTOS free evaluation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OSEK RTOS free evaluation?

6,807 Views
FC
Contributor III
Is OSEK RTOS free to evaluate? 
 
Besides FreeRTOS, is there any others available to evaluate?.  I would like to utilize an embedded os.
 
Thanks
Labels (1)
0 Kudos
Reply
3 Replies

2,128 Views
trolina
Contributor I
Try RTA-OSEK. Information is available at : http://en.etasgroup.com/products/rta/rta_osek_in_detail.shtml
0 Kudos
Reply

2,128 Views
mjbcswitzerland
Specialist V

Hi

You may like to look at the uTasker. It is an operating system with integrated TCP/IP stack - designed especially for single chip processors with embedded EMAC for IP control applications. [freescale MC9S12NE64 and M5223X are supported and projects can be moved between the two by simply setting one compiler switch]. Its most important feature is a real time chip simulator which allows complete embedded IP projects to be developed and tested on the PC (saving typically 60% of development time).

See the following posting for details and links to on-line demos:

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=274

The solution is free for educational and other non-commercial work (see licensing terms and application form in posting) - it can also be evaluated under this license agreement and free email support is included.

If you are not using the above chips it will probably work but will be a bit of a waste of its most powerful features. Support would then not be included.

Regards

Mark Butcher
www.mjbc.ch

 

0 Kudos
Reply

2,128 Views
J2MEJediMaster
Specialist I
There is NO free evaluation version of OSEKturbo, OSEKtime or AUTOSAR.

---Tom
0 Kudos
Reply