Not able to open Code Warrior IDE V8.8.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to open Code Warrior IDE V8.8.

872 次查看
harishg_ec
Contributor I

When the Code Warrior IDE is tried to Open, It is throwing Error as

 

"CodeWarrior Preferences File is read only or is currently in use"

 

Following Steps are done to remove error but error still exist

1. ProgramFiles/Codewarrior folder is made Read Write and tried to open

2. Restart the System and tried to Open

3. Uninstall and Install the Code Warrior, The error still exist.

 

Can you please suggest the method to make the code warrior work

 

Installation Setup

System -  Windows 7 (For Windows 7 Modification is done to enable the compatibility mode)

Code Warrior IDE - V 8.8

 

Thank you

Harish G

标签 (1)
0 项奖励
回复
1 回复

745 次查看
CrasyCat
Specialist III

Hello

 

   Windows 7 introduces some limitation on permission son folder located under Program Files.

  Can you please try the following:

      - Uninstall CodeWarrior

      - Install it outside of the Program Files folder (for instance in C:\Freescale)

 

CrasyCat

0 项奖励
回复