No uninstall for Codewarrior LE v4.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No uninstall for Codewarrior LE v4.0

3,978 Views
cmspaz
Contributor I
I can't uninstall codewarrior. There is no uninstall app in the codewarrior folder or the start menu group, the Add/Remove Programs window locks whenever I try to do it from there (probably becuase there's no unistall app for it to use), and the install app on the cd doesn't have an uninstall option, as most nowadays do.

I'm at wits end as to what to do, since I really don't want to just go in and delete everything manually. Too many fragments of the program would get left on the drive that way.

Any ideas as to what I can do?

I'm running XP Pro SP2, if that helps any.
Labels (1)
0 Kudos
Reply
3 Replies

2,198 Views
CrasyCat
Specialist III

Hello

  Which processor are you targeting (PowerPC, Coldfire, HC12, ...)?

CrasyCat

0 Kudos
Reply

2,198 Views
cmspaz
Contributor I
I'm not sure. How would I go about figuring this out?
0 Kudos
Reply

2,198 Views
CrasyCat
Specialist III

Hello

Is there a file called Welcome*.txt in your root installation directory?

You should see your target there...

CrasyCat

0 Kudos
Reply