NicheLite on Coldfire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NicheLite on Coldfire

2,136 Views
Ioanna
Contributor I

Hello,

 

i would like to implement an application with following features on a MCF52235 platform:

1. Webserver

2. Bootloader

3. Firmware Upgrade (FTP & File System)

4. TCPIP Stack

 

NicheLite seems to be a good option for that. Yet the documentation is very poor there. I have no example or guideline about FileSystem, Bootloader & Remote Upgrade.  Could somebody suggest me something.

 

Best regards, Ioanna

Labels (1)
0 Kudos
Reply
2 Replies

1,327 Views
TomLEE
Contributor III

Hello,

Forget InterNiche Lite Stack !!!

Use FNET (Freescale NET) developed by Mr Andrey Butok, the best world free stack for Ethernet communication with Freescale Microcontrollers.

Download it here : http://fnet.sourceforge.net

And see forum here : https://community.freescale.com/thread/57196?start=75&tstart=0

0 Kudos
Reply

1,327 Views
MCF52233
Contributor III

hi loanna,

 

nichelite already contains web-server n tcp/ip stack, but not firmware upgrade n bootloader.

Rather than u chk for uTasker which include all of this n it is free for educational purpose.

Also u can chk for fnet stack released recently includes all of this example n might be free.

0 Kudos
Reply