NicheLite on Coldfire

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NicheLite on Coldfire

2,133 次查看
Ioanna
Contributor I

Hello,

 

i would like to implement an application with following features on a MCF52235 platform:

1. Webserver

2. Bootloader

3. Firmware Upgrade (FTP & File System)

4. TCPIP Stack

 

NicheLite seems to be a good option for that. Yet the documentation is very poor there. I have no example or guideline about FileSystem, Bootloader & Remote Upgrade.  Could somebody suggest me something.

 

Best regards, Ioanna

标签 (1)
0 项奖励
回复
2 回复数

1,324 次查看
TomLEE
Contributor III

Hello,

Forget InterNiche Lite Stack !!!

Use FNET (Freescale NET) developed by Mr Andrey Butok, the best world free stack for Ethernet communication with Freescale Microcontrollers.

Download it here : http://fnet.sourceforge.net

And see forum here : https://community.freescale.com/thread/57196?start=75&tstart=0

0 项奖励
回复

1,324 次查看
MCF52233
Contributor III

hi loanna,

 

nichelite already contains web-server n tcp/ip stack, but not firmware upgrade n bootloader.

Rather than u chk for uTasker which include all of this n it is free for educational purpose.

Also u can chk for fnet stack released recently includes all of this example n might be free.

0 项奖励
回复