NicheLite on Coldfire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NicheLite on Coldfire

2,127件の閲覧回数
Ioanna
Contributor I

Hello,

 

i would like to implement an application with following features on a MCF52235 platform:

1. Webserver

2. Bootloader

3. Firmware Upgrade (FTP & File System)

4. TCPIP Stack

 

NicheLite seems to be a good option for that. Yet the documentation is very poor there. I have no example or guideline about FileSystem, Bootloader & Remote Upgrade.  Could somebody suggest me something.

 

Best regards, Ioanna

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,318件の閲覧回数
TomLEE
Contributor III

Hello,

Forget InterNiche Lite Stack !!!

Use FNET (Freescale NET) developed by Mr Andrey Butok, the best world free stack for Ethernet communication with Freescale Microcontrollers.

Download it here : http://fnet.sourceforge.net

And see forum here : https://community.freescale.com/thread/57196?start=75&tstart=0

0 件の賞賛
返信

1,318件の閲覧回数
MCF52233
Contributor III

hi loanna,

 

nichelite already contains web-server n tcp/ip stack, but not firmware upgrade n bootloader.

Rather than u chk for uTasker which include all of this n it is free for educational purpose.

Also u can chk for fnet stack released recently includes all of this example n might be free.

0 件の賞賛
返信