Need help,CodewarriorV3.2,debug error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help,CodewarriorV3.2,debug error

Jump to solution
3,238 Views
kyleden
Contributor I

 

OS 64bit-win7,

version CodeWarrior for 68K Embedded Systems v3.2,

when click the debug button,Error "Could not open fconfig file C\prgramfiles\metrowerks\codewarrior\E68Ksupport\Initialization_Files\M68360QUADS_PnE.cfg""

first time Develop the freescale MCU,,,thanks for help!

Labels (1)
0 Kudos
Reply
1 Solution
3,035 Views
trytohelp
NXP Employee
NXP Employee

Hi,

This interface is not supported.

The Multilink and Multilink FX interfaces were released may be 4 years ago.

CW for M68K V3.2 is supporting older version only based on Parallel on host interface.

For details please have a look to:

    http://cache.freescale.com/files/soft_dev_tools/doc/data_sheet/950-00038.pdf

Debugger Supports

> Codewarrior Target Resident Kernel debug monitor via serial

> BDM port for parallel interface from P&E Microsystems for CPU32

The P&E interface supported is:

    P&E Microcomputer Systems - CABLE_16/32 (Discontinued) - CPU16/3xx BDM Interface (5V, Parallel Port)...

Unfortunately this interface is not available anymore.

The Mulitlink FX replaces it but this is not supported by CW for M68K V3.2.

There is same problem with other older CW versions for HC12 and HC08.

P&E released some patches to solve the problem.

I know this is working for HC12  and HC08.

A patch for M68K is available but I don't know if this is working.

Please have a look to:

    P&E Microcomputer Systems


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,035 Views
trytohelp
NXP Employee
NXP Employee

Hi,

CW for M68K V3.2 is very old, released in 2002.

This version was designed for Win XP 32 bit OS.

To avoid problem we recommend to use XP OS.

What is the interface supported ?

Again this tool was released in 2002 so the interface supported are defined in the

\CodeWarrior_68K_3.2\CodeWarrior Manuals\PDF\Targeting_Embedded_68K_ColdFire.pdf manual.

Please have a look page 174.

    Serial - MetroTRK

    Ethernet - MetroTRK

    BDM - P&E Micro

    BDM - P&E Lightning

For details please have a look to:

    http://cache.freescale.com/files/soft_dev_tools/doc/data_sheet/950-00038.pdf

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,035 Views
kyleden
Contributor I

Hi,pascal

Thanks,

successfully installed in a XP OS。

I also installed version CodewarriorV5.0 for another development board。

but then the two version of codewarrior could not detect the Multilink Universal FX(P&E micro)...

The problem is really really more and more,haha

0 Kudos
Reply
3,036 Views
trytohelp
NXP Employee
NXP Employee

Hi,

This interface is not supported.

The Multilink and Multilink FX interfaces were released may be 4 years ago.

CW for M68K V3.2 is supporting older version only based on Parallel on host interface.

For details please have a look to:

    http://cache.freescale.com/files/soft_dev_tools/doc/data_sheet/950-00038.pdf

Debugger Supports

> Codewarrior Target Resident Kernel debug monitor via serial

> BDM port for parallel interface from P&E Microsystems for CPU32

The P&E interface supported is:

    P&E Microcomputer Systems - CABLE_16/32 (Discontinued) - CPU16/3xx BDM Interface (5V, Parallel Port)...

Unfortunately this interface is not available anymore.

The Mulitlink FX replaces it but this is not supported by CW for M68K V3.2.

There is same problem with other older CW versions for HC12 and HC08.

P&E released some patches to solve the problem.

I know this is working for HC12  and HC08.

A patch for M68K is available but I don't know if this is working.

Please have a look to:

    P&E Microcomputer Systems


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,035 Views
kyleden
Contributor I

Hi,Pascal

thank you very much!

I have install the two patches and successfully download program by Codewarrior5.0,

but failed in Codewarrior3.2, message"P&E BDM error!BDM returned an error message(0X100003c)".

I will check my PCBboard,

I will also ask PE micro for some help.

0 Kudos
Reply