Multiple target builds - PE suspended

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple target builds - PE suspended

2,167件の閲覧回数
JPB_plxs
Contributor I
Would like to build multiple project targets at once. Have done this with a non PE project, but would like to do it with a PE project. It complains that it can't do that, so...
 
I suspended PE. The PE tab went away. Tried the multiple target build again, and still it complains. How can I get this to work?
 

Message Edited by JPB_plxs on 2007-04-1908:52 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,011件の閲覧回数
trytohelp
NXP Employee
NXP Employee
If your application is using Processor Expert you can not build a multiple targets.
This is not supported.
Only one target can be build when Processor Expert is used.
Enable or disable Processor Expert will not change this restriction.
 
Regards
Pascal
 
0 件の賞賛
返信