MC56F8322 SCI Bootloader with Codewarrior Ver 5.2.1279

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8322 SCI Bootloader with Codewarrior Ver 5.2.1279

2,585件の閲覧回数
cwr_whitehead
Contributor I
I'm looking for the serial (SCI) bootloader code for the MC56F8322, that will work in Codewarrior ver 5.2.1279. Does anyone know where it can be found?
I need to change it to program the flash using SCI0 instead of SCI1.
Assuming I get and modify the code, do I just use Codewarrior Debug (JTAG) to program the boot flash?
 
Thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,252件の閲覧回数
cwr_whitehead
Contributor I
I've downloaded Codewarrior ver 8 and updated to Ver 8.1
 
Found the Bootloader code, modified and built fine. My problem now is that whenever I try to use Codewarrior debug I get the following error. 
 
CCS ProtocolPlugin : CCS: Command Convertor not present. 
 
Can anyone help.
0 件の賞賛
返信