Linker

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linker

1,591件の閲覧回数
VIPOFE
Contributor I

How can I use the linker to place a variable in a specific location in ROM?  I'm using a bootloader and would like for the application code to be able to read the bootloader version number etc...

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,183件の閲覧回数
CrasyCat
Specialist III

Hello

 

  - Which CPU are you targeting (HC08, HC12, Coldfire, ..)
  - Which version of CodeWarrior are you using?

To retrieve that info:
  - Start CodeWarrior
  - Select Help -> About Freescale CodeWarrior
  - Click on "Install Products"
  - CodeWarrior version used is displayed on top in the Installed Products dialog.

 

CrasyCat

 

0 件の賞賛
返信

1,183件の閲覧回数
J2MEJediMaster
Specialist I

I would try the search function at the upper right hand section of this page. Type in "variable at address" or something similar, change the menu coice from Board to Community, then click Search. I got a lot of hits. Some of them may be relevant to what you need. I cannot be any more specific because you did not mention what target you were developing for.

 

---Tom

0 件の賞賛
返信