Linker padding for SRec generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linker padding for SRec generation

3,052 Views
admin
Specialist II
Hello

dose anybody of you know what the DSC56800/e 8.2.2 linker error message
"Linker padding for SRec generation"
mean.

Thanks in advance.
Martin
Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,241 Views
FTSolutions
Contributor III
It is not an 'error' message, but more of an informative one.  you can turn off this feature from one of the settings in the linker setups.   I think that all it is indicating is that it is adding some "pad" bytes of 0x00 to fill out a full S-Record, fox example, if a variable array has 3 elements, and another structure is allocated a few words/bytes higher, the linker could simply generate one S-Record that contained both data elements with "0x00" pad values in between - simply for expediency/optimization purposes.

I might be wrong in this example, but I think this is what it is.

0 Kudos
Reply